RH850/U2Bx Selected type name in debugger
RH850/U2Bx Selected type name in debugger (FCC device)
The device selection name when using the debugger (CS+) is shown below.
When using the debugger, select the name listed in the Selected Name column.
| |
UM Product Name (representative) |
Package |
DF Filename |
Name of choice in CS+ |
| R7F702Z22EDBB |
U2B6-FCC |
FCBGA-292 |
DR7F702Z22.DVF |
R7F702Z22(XXXX) |
R7F702Z21EDBG R7F702Z21EDBA R7F702Z21EDBB |
U2B10-FCC |
FCBGA-468 FCBGA-373 FCBGA-292 |
DR7F702Z21.DVF |
R7F702Z21(Performance) |
R7F702Z26EDBG R7F702Z26EDBA R7F702Z26EDBB |
FCBGA-468 FCBGA-373 FCBGA-292 |
DR7F702Z26.DVF |
R7F702Z26(FuSa) |
R7F702Z23EDBG R7F702Z23EDBA |
U2B24-FCC |
FCBGA-468 FCBGA-373 |
DR7F702Z23.DVF |
R7F702Z23(Performance) |
R7F702Z28EDBG R7F702Z28EDBA |
FCBGA-468 FCBGA-373 |
DR7F702Z28.DVF |
R7F702Z28(FuSa) |
| note: In CS+ V8.08.00, "pin" are indicated |
|
|
RH850/U2Bx Selected type name in debugger (mass production)
The device selection name when using the debugger (CS+) is shown below.
When using the debugger, select the name listed in the Selected Name column.
| |
UM Product Name (representative) |
Package |
DF
Filename |
Name of choice in CS+ |
| R7F70255*FABB-C |
U2B6 |
BGA-292 |
DR7F70255x.DVF |
R7F70255x(XXXX) |
| R7F70255*AFABB-C |
| R7F70255*BFABB-C |
R7F70254*FABG-C
R7F70254*FABA-C
R7F70254*FABB-C |
U2B10 |
FCBGA-468
FCBGA-373
FCBGA-292 |
DR7F70254x_P.DVF |
R7F70254x(Performance) |
| R7F70254*AFABG-C |
FCBGA-468
|
| R7F70254*AFABA-C |
FCBGA-373
|
| R7F70254*AFABB-C |
FCBGA-292 |
R7F70254*FABG-C
R7F70254*FABA-C
R7F70254*FABB-C |
FCBGA-468
FCBGA-373
FCBGA-292 |
DR7F70254x_F.DVF |
R7F70254x(FuSa) |
| R7F70254*AFABG-C |
FCBGA-468
|
| R7F70254*AFABA-C |
FCBGA-373
|
| R7F70254*AFABB-C |
FCBGA-292 |
note: In CS+ V8.08.00, "pin" are indicated
DR7F70255xA.DVF has been merged into DR7F70255x.DVF. |
|
|