Differences with help information provided by the online help system
This page informs differences between information in the online help system and in user's manuals for CS+ or the offline help system
V8.14.00 (2025/7/22)
Build Tool Operation (CC-RX)
In the (2)[CPU], the [Instruction-set architecture] property is changed to "Changes not allowed".
In the (2)[CPU], the [Microcontroller type] property is changed to "Changes not allowed".
In the (2)[CPU], the Default and the display condition of the [Microcontroller type] property are amended.
In the (11)[Version Select], a remark is added to the [Using compiler package version] property.
WINDOW REFERENCE > Description > Property panel > [Library Generate Options]
In the (2)[Standard Library], the property name and the display condition of the [Enables wchar.h(C89/C99)] property are amended.
In the (2)[Standard Library], the property name and the display condition of the [Enables wctype.h(C89/C99)] property are amended.
License Manager
This help has been updated for the License Manager V2.09.00 release in October 2025.