1.1 Overview

The Code Generator, enables you to output the source code (device driver programs, C source files and header files) necessary to control the peripheral functions (clock generation circuit, voltage detection circuit, etc.) provided by the device by configuring various information using the GUI.