-preinclude


This option specifies the C header file that is included at the top of the compilation unit.

[Specification format]

-preinclude=file[,file]...

 

-

Interpretation when omitted

It is assumed that the file that is included at the top of the compilation unit does not exist.

[Detailed description]

-

This option specifies the file that is included at the top of the compilation unit as file.

-

If the file specified as file is not found, an error will occur.

[Example of use]

-

To include file "sample.h" at the top of the compilation unit, describe as:

>ccrl -preinclude=sample.h -cpu=S2 -dev=dr5f100pj.dvf main.c