3.3 Abort Errors

Table 3-3. Abort Errors

[Message]

Option (xxx) is not specified.

[Action by User]

Make sure whether the configuration file input to an option is specified.

[Message]

Cannot open device file.

[Action by User]

Make sure that the device file exists.

[Message]

File name (xxx) is duplicated.

[Message]

Option (xxx) needs parameters.

[Action by User]

Check the option.

[Message]

[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]

The parameters (xxx) is illegal.

[Action by User]

[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]

Check the parameter.

[Message]

[RI850MP]

Illegal parameters (xxx).

[Action by User]

[RI850MP]

Check the parameter.

[Message]

The option (xxx) is Illegal.

[Action by User]

Check the option.

[Message]

Illegal format is in command file.

[Action by User]

Check the contents of a command file.

[Message]

Path or file name is too long (xxx).

[Message]

File (xxx) is not a supported file to convert.

[Message]

A described device (xxx) is not supported.

[Message]

The size of the command (xxx) file is too big.

[Message]

Cannot open command file.

[Explanation]

The specified command file could not be opened. Otherwise, the specified command file name is not valid.

[Action by User]

Check whether the specified command file exists or whether the command file name is correct.

[Message]

[RI78V4 V1.xx.xx]

Usage:CF78V4 [@command file] [-i <SIT file> | -ni] [-dc <C header file> | -ndc] [-da <ASM header file> | -nda] [-V] [-help] <CF file>

[RI78V4 V2.xx.xx]

Usage: CF78V4 [@command file] [-cpu <Name>] [-devpath=<Path>] [-i <SIT file> | -ni] [-dc <C header file> | -ndc] [-da <ASM header file> | -nda] [-V] [-help] <CF file>

[Explanation]

Because the specified activation option is not correct, CF78V4 could not be executed.

[Action by User]

Check the activation option.

[Message]

Option (xxx) is multiple defined.

[Action by User]

Check the contents of a command file.

[Message]

Output file names are the same (xxx).

[Explanation]

The output files (system information table file, system information header file (for C language) or system information header file (for assembly languages)) are specified with the same file name "xxx".

[Action by User]

Check if the file names specified with the -i, -dc, and -da options are the same.

[Message]

It is necessary to specify the device file in the case of outputing entry file.

[Action by User]

Check the specified the output option of the entry file or the device file.

[Message]

It failed to convert file (xxx).

[Message]

Syntax too complecated.

[Action by User]

Check the description of the system configuration file.

[Message]

Unknown device file format.

[Action by User]

Check the device file.

[Message]

File read error (xxx).

[Explanation]

File (xxx) cannot be read.

[Action by User]

Check if the specified file exists. Alternatively, check whether the file name is correct or whether the file name is specified with the valid number of characters.

[Message]

File write error (xxx).

[Explanation]

File (xxx) could not be opened.

[Action by User]

Check whether the file is write-enabled or whether the disk is full. Alternatively, check if the number of characters for the specified file name or output file name converted to an absolute path is valid.

[Message]

[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]

Cannot execute Preprocessor.

[Action by User]

[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]

Check the pass of a preprocessor and the option.

[Message]

[RI850MP]

Cannot execute Preprocessor (xxx).

[Message]

Too many errors.

[Message]

File name has already existed (xxx).

[Message]

Not enough memory.

[Explanation]

The available memory is insufficient.

[Action by User]

The available memory is insufficient.

The available memory is insufficient to analyze the activation option/command file or to analyze the system configuration file. Increase the memory capacity available for CF78V4 by quitting any applications that are not in use.

[Message]

[RI850V4 V2.xx.xx]

PEID(xxx) is not defined in the device file.

[Explanation]

[RI850V4 V2.xx.xx]

The specified PEID(xxx) is not defined in the device file.

[Action by User]

[RI850V4 V2.xx.xx]

Check the PE number as specified "-peid" option.

[Message]

[RI850V4 V2.xx.xx]

Cannot read xxx in the device file.

[Explanation]

[RI850V4 V2.xx.xx]

Cannot read the information "xxx" from the device file.

[Action by User]

[RI850V4 V2.xx.xx]

Renews the latest device file or reconsiders the specified option.

[Message]

[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]

CF850V4 internal error (xxx).

[Action by User]

[RI850V4 V1.xx.xx] [RI850V4 V2.xx.xx]

Please contact your vendor or your Renesas Electronics overseas representative.

[Message]

[RI850MP]

CF850MP internal error (xxx).

[Action by User]

[RI850MP]

Please contact your vendor or your Renesas Electronics overseas representative.