Rebuilding a Program

Rebuild the program of loaded sample project.

1. Build project

In this step, rebuild the program of loaded sample project.

Click the [Rebuild Project.] button.

Check to see if the rebuild process has been completed

correctly. If the build process has been completed correctly,

a load module file is created.