Starting CS+

2. Load the sample project

In this step, load the sample project.

In the "Load Sample Project" field, from the "RX" tab, select " RH850_F1L_Tutorial_Basic_Operation ", then click [GO].

Follow the on-screen instructions. A sample program opens as shown in the figure below.