4. COMPONENT NUMBERS

This chapter describes the component number displayed by CS+.

 

The component number (2 digits) categories when CS+ is operated are as follows.

Table 4.1

Component Number

Component Number

Description

00

Common processing

01

Update Manager/Installer/License Manager

02

Integrated Development Environment Framework

03

Design Tool (Pin Configurator)

04

Design Tool (Code Generator)

06

Debug Tool (Emulator/Simulator)

08

Analyze Tool

12

Debug Tool (Emulator/Simulator)

13

Debug Tool (Simulator)

17

Console

18

Debug Tool

20

Editor

22

I/O header file Generation Tool

23

Solution