2.2 When Using RI600V4, RI600PX Configurator

The output format when RI600V4, RI600PX Configurator is operated is as follows.

(1) When the file name and line number are included

 file-name:(line-number) : message-number (message-type) message


(2) When the line number aren't included

 file-name:(0) : message-number (message-type) message


(3) When the file name and line number aren't included

 --------:(0) : message-number (message-type) message


Remarks 1. Following contents are output as the character string.

message-number: O + 4 digits
message-type: 1 alphabetic character


2. See "CubeSuite+ Message" for details about the message-type and the message-number.