1.2 Features

The following are the features of the debugger provided by CS+.

 

-

Synchronous execution and synchronous break in a microcontroller that supports multi-core
Synchronous execution and synchronous break are available when the target microcontroller supports multi-core.
Information regarding a desired core is displayed on the panel by switching the core selection.

 

-

Connecting to the various debug tools

A pleasant debugging environment for target systems is provided by connecting to the full-spec emulator (Full-spec emulator), the on-chip debugging emulator (E1/E20) and Simulator.

 

-

C source text and disassembled text are shown mixed

The C source text and the disassembled text are shown mixed on the same panel.

 

-

Source level debugging and instruction level debugging

The source level debugging and the instruction level debugging for a C source program can be done.

 

-

Support of flash self programming emulation (Code flash)

The code flash can be rewrote by using the flash self library of the flash self programming function.

 

-

Real-time display update function

The contents of memory, registers and variables are automatically updated not only when the program execution is stopped, but also in execution.

 

-

Save/restore the debugging environment

The debugging environment such as breakpoints, event configuration information, file download information, display condition/position of the panel, etc. can be saved.