Select the value of the SFR to edit in the [Value] area, then click on it again to switch the value to edit mode (press the [Esc] key to cancel the edit mode).
To write the edited value to the target memory, directly enter the value from the keyboard then press the [Enter] key.
If a number with fewer digits than the size of the SFR is entered, the higher-order digits will be padded with zeroes. |
If a number with more digits than the size of the SFR is entered, the higher-order digits will be masked. |