When the emulator system is initiated, it initializes the general registers and part of the control registers as shown in Table 2.33. The initial values of the microcontroller are undefined.
Bits 15 to 0 in the ACC register are always read as 0. Attempts at writing to those bits will be ignored. |
If register values are changed in the [CPU Register] panel, it is immediately before the user program starts running that the changes are actually reflected in the registers. The same applies when the Debugger.Register.SetValue command is used to change register values. If, after register values are changed in the [CPU Register] panel or with the Debugger.Register.SetValue command, the CPU is reset without executing the user program even once, the changed register values have no effect. |
When the emulator is used, release from power-down modes can be accomplished by a source for release or by pressing the [STOP] button, causing a break to occur.
If, while the user program remains halted, a reset is asserted by means of a pin reset, the reset signal is masked off during a JTAG connection. Note, however, that during a FINE connection, it is not masked and the microcontroller is reset.
Do not break the user program when the RES#, or WAIT# signal is being low. A TIMEOUT error will occur. If the WAIT# signal is fixed to low during break, a TIMEOUT error will occur at memory access. |
The DMAC operates even during breaks in execution. Therefore, when a data transfer request is generated, the DMAC executes DMA transfer. Also, refer to section 2.22.8 DMAC and DTC.
Counting by the watchdog timer is suspended during breaks in execution. When execution of the user program is restarted, the counting is also resumed.
Do not change the values of clock generator circuit-related registers while the user program is under execution. For details about the clock generator circuit-related registers, refer to the hardware manual for the microcontroller you’re using.
Even if a user program is not being executed (including when run-time debugging is being performed), timers and other peripherals do not stop running. If a maskable interrupt is requested when the user program is not being executed (including when runtime debugging is being performed), the maskable interrupt request cannot be accepted, because the emulator disables interrupts. The interrupt request is accepted immediately after the user program execution is started. |
Take note that when the user program is not being executed (including when run-time debugging is being performed), a peripheral I/O interruption is not accepted. |
The E1, E20, and EZ emulators transfer firmware to the FCU RAM when their system is started up.