R_ADC_Get_Result


Reads the results of A/D conversion (10 bits).

[Syntax]

#include    "r_cg_macrodriver.h"
void    R_ADC_Get_Result ( uint16_t * const buffer );

[Argument(s)]

I/O

Argument

Description

O

uint16_t  * const buffer;

Pointer to area in which to store read results of A/D conversion

[Return value]

None.