R_DOC_SetMode


Configures the operation mode of data operation circuit.

[Syntax]

#include     “r_cg_macrodriver.h”
#include     “r_cg_doc.h”
MD_STATUS     R_DOC_SetMode ( doc_mode_t mode, uint16_t value);

[Argument(s)]

I/O

Argument

Description

I

doc_mode_t  mode;

Operation mode of data operation circuit

ADDTION: Data addition mode

SUBTRACTION: Data subtraction mode

COMPARE_MATCH: Data comparison mode

(Detection Condition: Data match is detected)

COMPARE_MISMATCH: Data subtraction mode

(Detection Condition: Data mismatch is detected)

I

uint16_t  value;

Data addition and data subtraction : Results of operations

Data comparison : 16-bit data for use as a reference

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument specification