r_lvd_vddinterrupt


Performs processing in response to the voltage detection of VDD pin interrupt INTLVDVDD.

Remark

This API function is called as the interrupt process corresponding to the voltage detection of VDD pin interrupt INTLVDVDD.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_lvd_vddinterrup ( void );

 

CC-RL Compiler

static  void  __near r_lvd_vddinterrup ( void );

[Argument(s)]

None.

[Return value]

None.