R_OSDC_Set_PowerOff


Halts the clock supplied to the oscillation stop detector.

Remark

Calling this API function changes the oscillation stop detector to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

[Syntax]

void    R_OSDC_Set_PowerOff ( void );

[Argument(s)]

None.

[Return value]

None.