R_PGA_DSAD_Get_AverageResult


Reads the average results of A/D conversion.(mean value)

[Syntax]

#include    "r_cg_macrodriver.h"
void    R_PGA_DSAD_Get_AverageResult ( uint16_t * const bufferH, uint16_t * const bufferL );

[Argument(s)]

I/O

Argument

Description

O

uint16_t  * const bufferH;

Pointer to area in which to store read results of A/D conversion

(DSADMVM resister and DSADMVH resister)

O

uint16_t  * const bufferL;

Pointer to area in which to store read results of A/D conversion

(DSADMVC resister and DSADMVL resister)

[Return value]

None.