r_sg_interrupt


Performs processing in response to the threshold value detection of the logarithmic decrement interrupt INTSG.

Remark

This API function is called as the interrupt process corresponding to the threshold value detection of the logarithmic decrement interrupt INTSG.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_sg_interrupt ( void );

 

CC-RL Compiler

static  void  __near r_sg_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.