3. MESSAGE TYPES

This chapter describes the message types displayed by CS+.

 

The message types (1 alphabetic character) when CS+ is operated are as follows.

Table 3.1

Message Type

Message Type

Description

C

Internal error

Processing terminated (suspended) due to internal error.

E

Fatal error

Processing terminated (suspended) due to fatal error.

M

Information

Informational message. Check the message and continue the process.

Q

Choice

This type of message is displayed when a choice is necessary in order to carry on with the next operation. It performs the selected action.

W

Warning

Warning message. Check the message and continue the process.