2.5 Set Link Options

To set options for the link phase, select the Build tool node on the project tree and select the [Link Options] tab on the Property panel.

You can set the various link options by setting the necessary properties in this tab.

Caution

This tab is not displayed for the library project.

Remark

Often used options have been gathered under the [Frequently Used Options(for Link)] category on the [Common Options] tab.