2.6.2 Change output destination folder

The Code Generator is used to change the output destination folder for the report file by selecting [Code Generator Setting] tab >> [Generate File Mode] >> [Output folder] in the Property panel.

Figure 2.15

Change Output Destination Folder