Print Preview window


This window is used to preview the file currently being displayed in the Editor panel before printing.

Figure A.16

Print Preview Window

Remark

This panel can be zoomed in and out by moving the mouse wheel forward or backward while holding down the [Ctrl] key.

 

The following items are explained here.

[How to open]

-

Focus the Editor panel, and then select [Print Preview] from the [File] menu.

[Description of each area]

(1)

Preview area

This window displays a form showing a preview of how and what is printed.

The file name (fully qualified path) and the page number are displayed at the page header and page footer.

The display differs according to whether the debug tool is or is not connected, and when it is connected, to whether the display is in normal display mode or mixed display mode. Note, however, that columns that are hidden on the Editor panel are not displayed (these columns are not printed).

[Toolbar]

 

Opens the Print dialog box provided by Windows to print the current Editor panel as shown by the print preview form.

 

This button is always disabled.

 

Increases the size of the content.

 

Decreases the size of the content.

 

Displays the preview at 100-percent zoom (default).

 

Fits the preview to the width of this window.

 

Displays the whole page.

 

Displays facing pages.

[Context menu]

Increase Zoom

Increases the size of the content.

Decrease Zoom

Decreases the size of the content.