2.3 Canceling an update

From the Update in progress dialog box, click the [Cancel] button to cancel the update. If the update was canceled, then the Finish page will show that the update was canceled.

When performing an update, it is not possible to update currently running related tools or open files. For this reason, if a related tool is running then the installation will be postponed, and the Finish page will indicate that the installation was suspended.