[Category Information] tab


This tab shows the detailed information on the category node (the category that the user added), Files node, and Build tool generated files node categorized by the following and the configuration can be changed.

Note that if multiple source files exist under the category node (the category of files that the user added) or file node, the same type of tabs (e.g., [Individual Compile Options] tab and [Individual Assemble Options] tab) among the tabs for those source files are merged into a single tab. See the "CS+ Integrated Development Environment User’s Manual: Build Tool Operation" for details about tabs.

 

(1) [Category Information]

(2) [Notes]

[Description of each category]

(1)

[Category Information]

The detailed information on the category is displayed and the configuration can be changed.

Category name

Specify the name of the category to categorize files.

This property of the Files node and Build tool generated files node is displayed in gray and you cannot change the attribute.

Default

Category name of files

How to change

Directly enter in the text box.

Restriction

1 to 200 characters

Shortcut to a folder

Specify a shortcut to a folder.

If a relative path is specified, the reference point of the path is the main project or subproject folder.

This property of the Files node and Build tool generated files node is not displayed.

Default

Blank

How to change

Directly enter in the text box or edit by the Browse For Folder dialog box which appears when clicking the [...] button.

Restriction

Up to 247 characters

(2)

[Notes]

The detailed information on notes is displayed and the configuration can be changed.

This category of the Files node and Build tool generated files node is not displayed.

Memo

Add memos to the category of files.

Add one item in one line.

The specified memo is displayed as the subproperty.

Default

Memo[number of items]

How to change

Edit by the Text Edit dialog box which appears when clicking the [...] button.

For the subproperty, you can enter directly in the text box.

Restriction

Up to 256 characters

Up to 256 items can be specified.