Everything
2.6.3 Remove a file from the build target

You can remove the specific file from the build target out of all the files added to the project.

Select the file to be removed from the build target on the project tree and select the [Build Settings] tab on the Property panel.

Select [No] on the [Set as build-target] property in the [Build] category.

Figure 2.56

[Set as build-target] Property

Remark

The files that this function can be applied to are C source files, assembly source files, object files, and library files.