Everything
2.9.4 Close a project

To close a project, select the [File] or [Project] menu >> [Close Project].

Figure 2.104

[Close Project] Item

 

When the open project or changed files are not saved, a Message dialog box is displayed.

Figure 2.105

Message Dialog Box

 

Click the [Yes] button to save, click the [No] button to not save.

Caution

If you have changed build options prior to building and close a project without saving it, the build options in the project file may not match the contents of the load module. Be sure to save a project before closing it if you have changed build options.