Everything

-preinclude


< Compile Options / Source Options >

[Format]

-preinclude=<file name>[,...]

[Description]

-

This option includes the specified file contents at the head of the compiling unit.

-

If the file name is specified by its relative path, the folder is searched in the following order:

-

[V3.01.00 or earlier]

-

Folder with the compilation unit

-

Folder specified by the include option

-

Folder specified by environment variable INC_RX

-

[V3.02.00 or later]

-

Folder that started the compiler

-

Multiple file names can be specified by separating them with a comma (,).

[Remarks]

-

If this option is specified for more than one time, all specified files will be included.