Everything

-subcommand


< Compile Options / Other Options >

[Format]

-subcommand=<subcommand file name>

[Description]

-

When the subcommand option is specified, the compiler options specified in a subcommand file are used at compiler startup. Specify options in a subcommand file in the same format as in the command line.

[Remarks]

-

If this option is specified for more than one time, all specified subcommand files are valid.