Everything
 

Pseudo-Error Debugging panel [Full-spec emulator][E1][E20]


This panel is central to the functionality of the solution for pseudo-error debugging.

See "2.23 Pseudo-error Debugging [Full-spec emulator][E1][E20]" for details on the solution for pseudo-error debugging.

Figure A.56

Pseudo-Error Debugging Panel

 

This section describes the following.

[How to open]

-

From the [Debug] menu, select [Debug Solutions] >> [Pseudo-Error Debugging].

-

On the Solution List panel, click the [Go] button of Pseudo-error debugging.

[Description of each area]

(1)

Pseudo-error list area

This area lists pseudo-errors which are targets in pseudo-error debugging.

The full name of a pseudo-error is displayed by hovering the mouse cursor over the node of each pseudo-error.

Each item is explained as follows:

(a)

Check box

When a check box is selected, this pseudo-error is generated after pseudo-error debugging starts.

(b)

Occurred

This column shows whether this pseudo-error has been generated when the debugger is stopped.

"!" is displayed if the pseudo-error has been generated and nothing is displayed if it has not been generated.

Remark

For RH850/G4MH devices, the number of occurrences of a pseudo-error that can be counted is up to three. If the corresponding pseudo-error occurs more times than this, "!" will be displayed as the counted number of times the pseudo-error occurred.

(c)

Error Name

The abbreviated name of this pseudo-error is displayed.

(d)

Bit Name

The bit name of IOR that triggers the generation of this pseudo-error is displayed.

(2)

[Breakpoint List]

A list of breakpoints that are to be used for pseudo-error debugging is displayed.

Only the breakpoints whose check box is selected will be valid for pseudo-error debugging.

Either of the following icons is displayed at the beginning of each breakpoint.

 

Breakpoint is valid.

 

Breakpoint is invalid.

[Toolbar]

 

Starts pseudo-error debugging based on the settings made in this panel.

 

Has the same functionality as the same button on the Debug toolbar in the Main window.

 

Opens the Select Pseudo-Error dialog box [Full-spec emulator][E1][E20] used to select ECM pseudo-errors that are targets of pseudo-error debugging.

 

Clears the error status of all pseudo-errors.

 

Opens the Breakpoint Setting dialog box [Full-spec emulator][E1][E20] to add a breakpoint.

 

Deletes breakpoints selected in [Breakpoint List].