Everything
2.10 Set Multi-core Project

As a multi-core project, set information on the individual application projects related to the boot loader project in the boot loader project.

Afterwards, the application projects are automatically built and associations with the addresses of the symbols this produces are set up whenever you debug the boot loader project, which eases debugging. The hex files generated from the individual projects are also combined in a single file.

See “2.10.1Set the constituent application projects” for details about setting up the associations. See “2.10.2Combine multiple objects” for details about producing a combined hex file.

Caution

Changing the microcontroller for a project will disable the settings specified in the [Constituent application projects] property for the [Constituent Projects] category on the [Boot Loader] tabbed page. To change the microcontroller while retaining the associations, select multiple related projects in the Project Tree panel.