Everything
4.2 Message Types

The message types are classified as follows.

Table 4.1

Message Types

Message Type

First Letter

Description

Internal error

C

Processing is aborted.

The C source program is not output after conversion.

Fatal Error

E

Processing is aborted.

The C source program is not output after conversion.

Warning

W

Processing continues.

The C source program is output after conversion.

Information

M

Processing continues.

The C source program is output after conversion.