Everything
2.1 Installing License Manager

Install the license manager which is included in the installer for the CS+ IDE, or with a package for a stand-alone language tool.

 

The preparing for installation window automatically appears. If this does not happen, double-click on “Setup.exe” in the root directory of the CD.

Caution

The floating license client setup must be conducted with administrator privileges.