Everything
3.1 Changing Active Project

If you change the active project, it is possible that nothing will be shown in the Function List panel/Variable List panel/Call Graph panel/Class/Member panel, because no cross reference file has been generated.

If this happens, rebuild after setting the [Enable static analysis information] property in the [General] category on the [Settings] tab of the Property panel to [Yes]. The contents of the panel will be updated.