Everything
 

Filter Settings dialog box


This dialog box is used to set the filter conditions when filtering the display of analysis information on the Function List panel/Variable List panel.

Caution

The filtering configured via this dialog box and the Filtering results linked to panel are mutually exclusive functions.
For this reason, the two filtering functions here cannot be enabled simultaneously (when one of the filters is active, setting the other filter will disable all filters set to date).
See "2.6.5Filter the analysis information" for details on the display-filter.

Figure A.44

Filter Settings Dialog Box

 

The following items are explained here.

[How to open]

-

On the Function List panel/Variable List panel, click the filter icon ( / ), and then select the [(Custom)].

[Description of each area]

Configure the filter conditions.

In the First condition setting area (top)/Second condition setting area (bottom), you can specify up to two conditions. Use the Logical operator buttons ([AND]/[OR]) to set the two conditions as a single filter condition.

(1)

First condition setting area (top)/Second condition setting area (bottom)

(a)

Comparison value (left combo box)

You can either type the comparison value of for the filter (number or string) directly via the keyboard (up to 2048 characters), or select one from the input history via the drop-down list (maximum 10 items).

By default, the comparison value set in the current target item is displayed.

(b)

Condition (right combo box)

Select the condition for the comparison value specified in (a) above, from the drop-down list.

By default, the condition set in the current target item is selected.

Item

Comparison Value

Numerical Value

Character String

no conditionNote

Compared as numerical value

Compared as character string

equals

does not equal

is greater than

is greater than or equal to

is less than

is less than or equal to

begins with

Compared as character string

does not begin with

ends with

does not end with

contains

does not contain

Note

If [no condition] is selected, then the comparison value will be ignored (not set as a condition).

Caution

Use the top condition-specification area if you only wish to specify one filtering condition.

(2)

Logical operator buttons

Select the logical relationship holding between the conditions specified in the First condition setting area (top)/Second condition setting area (bottom) via the following option button.

AND

Only information meeting both condition 1 and condition 2 is displayed.

This is mutually exclusive to the [OR] button.

OR

Only information meeting either condition 1 or condition 2 is displayed.

This is mutually exclusive to the [AND] button.

[Function buttons]

Button

Function

OK

Displays the analysis information in the Function List panel/Variable List panel under the specified filtering conditions.

If the Filtering results linked to panel was performed, then all display-filters linked to the panel conducted prior to this are deleted.

Cancel

Ignores the setting and closes this dialog box.

Help

Displays the help of this dialog box.