Everything
 

Section Address dialog box


This dialog box is used to set an address when adding or modifying a section.

Figure A.8

Section Address Dialog Box

 

The following items are explained here.

[How to open]

-

On the Section Settings dialog box, select an address in the address-section area, and then click the [Add...] or [Modify...] button.

[Description of each area]

(1)

[Address]

Specify the start address of the section.

Directly enter the address in the text box or select from the button.

The range that can be specified for the value is 0 to FFFFFFFF (hexadecimal number) (default: 0).

[Function buttons]

Button

Function

OK

-

When opening from the [Add...] button in the Section Settings dialog box

Closes this dialog box and adds the specified address to an appropriate location in the address-section area in the Section Settings dialog box (the section column remains empty).

-

When opening from the [Modify...] button in the Section Settings dialog box

Closes this dialog box and moves the section group (an address and the sections allocated to the address) to an appropriate location in the address-section area in the Section Settings dialog box.

Cancel

Cancels the settings and closes this dialog box.

Help

Displays the help of this dialog box.