Everything

APPENDIX A WINDOW REFERENCE


This appendix explains the window/panels that are used when the activation option for the CF78V4 is specified from the integrated development environment platform "CS+".
A.1 Description
The following shows the list of window/panels.
Table A-1 List of Window/Panels
Window/Panel Name
Function Description
This is the first window to be open when the CS+ is launched.
This panel is used to display the project components in tree view.
This panel is used to display the detailed information on the Realtime OS node, system configuration file, or the like that is selected on the Project Tree panel and change the settings of the information.