Everything
2.13.1 Display call stack information

Call stack information is displayed in the Call Stack panel below.

Select the [View] menu >> [Call Stack].

For details on the contents and function in each area, see the section for the Call Stack panel.

Caution

Nothing is displayed on this panel during execution of a program.
When the program is stopped, items in each area are displayed.

Figure 2.59

Display Call Stack Information (Call Stack Panel)

This section describes the following.

 

2.13.1.1 Change display format of values

2.13.1.2 Jump to the source line

2.13.1.3 Display local variables

2.13.1.4 Save the contents of call stack information