Everything
2.11.1 Display call stack information

Call stack information is displayed in the Call Stack panel below.

Select the [View] menu >> [Call Stack].

For details on the contents and function in each area, see the section for the Call Stack panel.

Caution

Nothing is displayed on this panel during execution of a program.
When the program is stopped, items in each area are displayed.

Figure 2.67

Display Call Stack Information (Call Stack Panel)

(1): [Depth] area

(2): [Call Stack] area

 

This section describes the following.

 

2.11.1.1 Change display format of values

2.11.1.2 Jump to the source line

2.11.1.3 Display local variables

2.11.1.4 Save the contents of call stack information