Everything
 

Customize dialog box


This dialog box is used to set or change the color and fonts for the Signal Data Editor window, Timing Chart window or Serial window.

Figure A.60

Customize Dialog Box: [Color] Tab (For Timing Chart Window)

Figure A.61

Customize Dialog Box: [Font] Tab

 

This section describes the following.

[How to open]

-

With the Signal Data Editor window, Timing Chart window or Serial window in focus, select [Customize...] from the [Option] menu.

[[Color] tab]

(1)

Color setting area

Set and change the color of each part in the window.

List

The parts for which color change is possible are displayed in list form.

The parts displayed differ depending on the target window.

Color

The currently set color of the part is displayed when that part is selected from the list.

[Change...] button

The color currently set for the relevant part of each listed item can be changed.

[[Font] tab]

(2)

Font setting area

Set and change the text font of each part in the window.

List

The parts for which font change is possible are displayed in list form.

Font

The current font name of the part is displayed, when that part is selected from the list.

Size

The current font size of the part is displayed, when that part is selected from the list.

[Change...] button

The font currently set for the relevant part of each listed item can be changed.

[Function buttons]

Button

Function

OK

Validates the settings and closes this dialog box.

Cancel

Cancels the settings and closes this dialog box.

Apply

Cannot be selected.

Help

Displays the help for this dialog box.