Everything
2.14.2.1 Checking the status bar for confirmation

When a program has stopped running, the measurement result is displayed in the status bar on the Main window (While no measurements are made, this status shows "Not measured").

Figure 2.137

Example of a Run-Break Timer Event Measurement Result (Status Bar)