Everything
2.12.1.4 Saving the displayed contents of call stack information

Selecting [Save Call Stack Data As...] from the [File] menu will open the Save As dialog box in which you can save the entire call stack information either in a text file (*.txt) or a CSV file (*.CSV) format. When saving to a file, the latest information will be retrieved from the debug tool.

Figure 2.123

Call Stack Information Output Image When Saved