Everything
2.9 Execute Programs

This section describes how to execute programs.

The major operations discussed in this section can be conducted either from the debug toolbar or the [Debug] menu in the Main window, where commands to control the execution of programs are included.

Caution

Items in the debug toolbar and the [Debug] menu will be disabled once the connection with the debug tool is lost.

Figure 2.87

Debug Toolbar

Figure 2.88

[Debug] Menu