Everything
2.11.5.1 Changing the form in which values are displayed

The form in which the data in the [Value] area are displayed can be freely changed using the toolbar buttons shown below.

Notation

Shows the following buttons that change the form in which values are displayed.

 

AutoSelect

Displays values on this panel in per-variable predetermined notation (default).

Hexadecimal

Displays values on this panel in hexadecimal.

Decimal

Displays values on this panel in decimal.

Octal

Displays values on this panel in octal.

Binary

Displays values on this panel in binary.

Decimal Notation for Array Index

Displays array indexes on this panel in decimal (default).

Hexadecimal Notation for Array Index

Displays array indexes on this panel in hexadecimal.

Float

Displays values on this panel in Float.

Except for 4-byte data or when values have type information, however, they are displayed in predetermined notation.

Double

Displays values on this panel in Double.

Except for 8-byte data or when values have type information, however, they are displayed in predetermined notation.

 

Adds a hexadecimal equivalent for the displayed value at the end of it, with the equivalent enclosed in parentheses ( ).

Encoding

Shows the following buttons that change the encoding in which string variables are displayed.

 

ASCII

Displays string variables in ASCII code (default).

Shift_JIS

Displays string variables in Shift_JIS code.

EUC-JP

Displays string variables in EUC-JP code.

UTF-8

Displays string variables in UTF-8 code.

UTF-16 Big-Endian

Displays string variables in UTF-16 Big-Endian code.

UTF-16 Little-Endian

Displays string variables in UTF-16 Little-Endian code.

UTF-32 Big-Endian

Displays string variables in UTF-32 Big-Endian code.

UTF-32 Little-Endian

Displays string variables in UTF-32 Little-Endian code.