Everything
B.3.10 CS+ Python property (for debug tool)

Below is a list of CS+ Python properties (for the debug tool).

Table B.10

CS+ Python Property (For Debug Tool)

Property Name

Function Description

debugger.ActionEvent.GetLine

This property sets or refers to the number of action event results.

debugger.ADConvertDataInExecution

This property sets or refers to data collected in debugging.

debugger.DebugTool.SerialNumber

This property sets or refers to the serial number of the emulator.

debugger.DebugTool.SerialNumberList

This property refers to the list of serial numbers of emulators.

debugger.Download.Property

This property sets or refers to conditions of the download file of the debug tool.

debugger.Interrupt.ExceptionCause

This property refers to the exception cause code.

debugger.IsMulticore

This property checks whether or not the microcontroller of the active project is multi-core.

debugger.Memory.NoVerify

This property switches the write-time verification setting.

debugger.Option.AccessDuringExecution

debugger.Option.AccessStopExecution

debugger.Option.AccumulateTraceTime

debugger.Option.AfterTraceMemoryFull

debugger.Option.Coverage

debugger.Option.CpuEndian

debugger.Option.MainClockFrequency

debugger.Option.OpenBreak

debugger.Option.ResetMask

debugger.Option.ReuseCoverageData

debugger.Option.SupplyPower

debugger.Option.SupplyPowerVoltage

debugger.Option.Timer

debugger.Option.Trace

debugger.Option.TraceBranchPC

debugger.Option.TraceDataAccess

debugger.Option.TracePriority

debugger.Option.TraceTarget

debugger.Option.UseTraceData

This property sets or refers to the options of the debug tool.

debugger.ProcessorElement

This property sets or refers to the PE of the multi-core.

debugger.ProcessorElementName

This property sets or refers to the PE of multiple cores with the name.

debugger.SoftwareTraceLPD.PEList

This property refers to a list of PE numbers for which software tracing (LPD output) is available.

debugger.SoftwareTraceLPD.Priority

This property sets or refers to the priority for the acquisition of software trace (LPD output) data.

debugger.SoftwareTraceLPD.RecordingMode

This property sets or refers to the operation of the debug tool when the memory for recording software trace information (LPD output) becomes full.

debugger.XTrace.Addup

debugger.XTrace.Complement

debugger.XTrace.Mode

This property sets or refers to the tracing options of the debug tool.