CS+ enables the execution of IronPython functions and control statements, and CS+ Python functions (see "B.3 CS+ Python Function/Class/Property/Event") added for controlling CS+ via command input method.
Select [Python Console] from the [View] menu and select the [Console] tab on the Python Console panel.
You can control CS+ and the debugging tool by executing Python functions and control statements in the panel.

See "B. Python CONSOLE/Python FUNCTIONS" for details about the Python console and Python functions. |