Logical product (immediate).
[Syntax]
The following can be specified for imm:
- | Absolute expression having a value of up to 32 bits |
- | Either of the above expressions with HIGHW, LOWW, or HIGHW1 applied |
[Function]
ANDs the value of the absolute expression, relative expression, or expression with HIGHW, LOWW, or HIGHW1 applied specified by the first operand with the value of the register specified by the second operand, and stores the result into the register specified by the third operand.
[Description]
- | If the following is specified as imm, the assembler generates one andi machine instructionNote 1. |
(a) | Absolute expression having a value in the range of 0 to 65,535 |
andi imm16, reg1, reg2
|
andi imm16, reg1, reg2
|
(b) | Relative expression having !label or %labelNote 2 |
andi !label, reg1, reg2
|
andi !label, reg1, reg2
|
andi %label, reg1, reg2
|
andi %label, reg1, reg2
|
(c) | Expression with HIGHW, LOWW, or HIGHW1 |
andi imm16, reg1, reg2
|
andi imm16, reg1, reg2
|
Note 1. | The andi machine instruction takes an immediate value of 0 to 65,535 (0 to 0xFFFF) as the first operand. |
Note 2. | !label and %label are treated as 16-bit value (zero-extended). |
- | If the following is specified for imm, the assembler executes instruction expansion to generate multiple machine instructions. |
(a) | Absolute expression having a value in the range of -16 to -1 |
If reg2 is r0
andi imm5, reg1, r0
|
mov imm5, r1
and reg1, r1
|
Else if reg2 is the same as reg1
andi imm5, reg1, reg2
|
mov imm5, r1
and r1, reg2
|
Else
andi imm5, reg1, reg2
|
mov imm5, reg2
and reg1, reg2
|
(b) | Absolute expression having a value in the range of -32,768 to -17 |
If reg2 is r0
andi imm16, reg1, r0
|
movea imm16, r0, r1
and reg1, r1
|
Else if reg2 is the same as reg1
andi imm16, reg1, reg2
|
movea imm16, r0, r1
and r1, reg2
|
Else
andi imm16, reg1, reg2
|
movea imm16, r0, reg2
and reg1, reg2
|
(c) | Absolute expression exceeding the above ranges |
<1> | If all the lower 16 bits of the value of imm are 0 |
If reg2 is r0
andi imm, reg1, r0
|
movhi HIGHW(imm), r0, r1
and reg1, r1
|
Else if reg2 is the same as reg1
andi imm, reg1, reg2
|
movhi HIGHW(imm), r0, r1
and r1, reg2
|
Else
andi imm, reg1, reg2
|
movhi HIGHW(imm), r0, reg2
and reg1, reg2
|
If reg2 is r0
andi imm, reg1, r0
|
mov imm, r1
and reg1, r1
|
Else if reg2 is the same as reg1
andi imm, reg1, reg2
|
mov imm, r1
and r1, reg2
|
Else
andi imm, reg1, reg2
|
mov imm, reg2
and reg1, reg2
|
(d) | Relative expression having $label for a label having a definition in the sdata/sbss-attribute section |
If reg2 is r0
andi $label, reg1, r0
|
movea $label, r0, r1
and reg1, r1
|
Else if reg2 is the same as reg1
andi $label, reg1, reg2
|
movea $label, r0, r1
and r1, reg2
|
Else
andi $label, reg1, reg2
|
movea $label, r0, reg2
and reg1, reg2
|
(e) | Relative expression having #label or label, or that having $label for a label having no definition in the sdata/sbss-attribute section |
If reg2 is r0
andi #label, reg1, r0
|
mov #label, r1
and reg1, r1
|
andi label, reg1, r0
|
mov label, r1
and reg1, r1
|
andi $label, reg1, r0
|
mov $label, r1
and reg1, r1
|
Else if reg2 is the same as reg1
andi #label, reg1, reg2
|
mov #label, r1
and r1, reg2
|
andi label, reg1, reg2
|
mov label, r1
and r1, reg2
|
andi $label, reg1, reg2
|
mov $label, r1
and r1, reg2
|
Else
andi #label, reg1, reg2
|
mov #label, reg2
and reg1, reg2
|
andi label, reg1, reg2
|
mov label, reg2
and reg1, reg2
|
andi $label, reg1, reg2
|
mov $label, reg2
and reg1, reg2
|
[Flag]
|
CY
|
---
|
|
OV
|
0
|
|
S
|
1 if the word data MSB of the result is 1, 0 if not
|
|
Z
|
1 if the result is 0, 0 if not
|
|
SAT
|
---
|