11.2 V850E3v5 G3K Core Specification for Assembler (-Xcpu=g3k Option)
The following instruction sets cannot be specified.
- | Hardware multithreading feature instructions |
- | Virtualization support feature instructions |
- | MMU control instructions |
- | Floating-point operation instructions |
The above instruction sets cause assemble errors when the V850E3v5 G3K core is specified. If any of them is specified, the assembler outputs the following message.
|
E0550269 : Illegal mnemonic(cannot use this mnemonic ins RH850 "G3K" core).
|