|
Flash Options Setting dialog box
|
This dialog box is used to configure options for the flash memory incorporated in the microcontroller.
Caution 1. | [Full-spec emulator][E1][E20]
This dialog box appears only when connecting to the debug tool.
[Simulator]
This dialog box appears only when disconnecting from the debug tool. |
Caution 2. | [Full-spec emulator][E1][E20]
CPU reset may be generated automatically when you click the [Write] button after changing the configuration of this dialog box. |
Figure A.33 | Flash Options Setting Dialog Box [Full-spec emulator][E1][E20] |
Figure A.34 | Flash Options Setting Dialog Box [Simulator] |
This section describes the following.
[How to open]
[Description of each area]
(1) | [Flash option property] area |
(a) | [Option Bytes Setting] |
You can configure the option bytes for the flash memory.
|
OPBT0 - 15
|
Specify the option bytes.
|
|
Default
|
The initial value stored in the device file.
|
|
Modifying
|
Directly enter from the keyboard.
|
|
Available values
|
0x0 to 0xFFFFFFFF in hexadecimal number
|
Caution | The number of option bytes (OPB0 - 15) to be displayed differs with the selected microcontroller (the bytes for some numbers might actually be unused). |
[Function buttons]
|
|
|
|
Read
[Full-spec emulator][E1][E20]
|
Reads the values currently specified in the debug tool, and reflects them in this dialog box.
|
|
Write
[Full-spec emulator][E1][E20]
|
Writes the currently set values in this dialog box to the debug tool, and reflects them in the project. Then, closes this dialog box.
|
|
Close
|
Specifies the currently set values in this dialog box to the project and closes this dialog box.
|
|
Cancel
|
Closes this dialog box without setting.
|
|
Help
|
Displays the help for this dialog box.
|