The display format of the address area/memory value area/character strings area can be changed using buttons below on the toolbar.
|
The following buttons to change the notation of memory values are displayed. |
||
|
The following buttons to change the notation of sizes of memory values are displayed. |
||
|
Displays memory values in 16-bit width. Values are converted depending on the endian of the target memory area. |
||
|
Displays memory values in 32-bit width. Values are converted depending on the endian of the target memory area. |
||
|
Displays memory values in 64-bit width. Values are converted depending on the endian of the target memory area. |
||
|
The following buttons to change the encoding of character strings are displayed. |
||
|
Displays character strings as a half-precision floating-point value. |
||
|
Displays character strings as a single-precision floating-point valueNote. |
||
|
Displays character strings as a double-precision floating-point valueNote. |
||
|
Displays character strings as a complex number of single-precision floating-pointNote. |
||
|
Displays character strings as a complex number of double-precision floating-pointNote. |
||
|
Displays character strings as an imaginary number of single-precision floating-pointNote. |
||
|
Displays character strings as an imaginary number of double-precision floating-pointNote. |
||
|
The following buttons to change the display format are displayed. |
||
|
Opens the Scroll Range Settings dialog box to set the scroll range for this panel. |
||
|
Opens the Column Number Settings dialog box to set the number of view columns in the memory value area. |
||
|
Opens the Address Offset Settings dialog box to set an offset value for addresses displayed in the address area. |
||
For details on the display of a floating-point value, see the section for the Memory panel. |