This chapter describes the output formats of messages.
 
The output format when CS+ is operated is as follows.
| 
(1) | When the file name and line number are included | 
| file-name (line-number) : message-type component-number message-number : message | 
| 
(2) | When the file name and line number aren't included | 
| message-type component-number message-number : message | 
| 
Remark | Following contents are output as the continued character string. | 
MESSAGE TYPES														:	1 alphabetic character
COMPONENT NUMBERS														:	2 digits
MESSAGE NUMBERS														:	5 digits